Hi,
I am designing a circuit using two stages of LMH6629 with +/-2.5V supply to amplify the signal from a "Silicon Photomultiplier" optical sensor. The typical signals of interest will be 1-10 mV, however rare signals up to 7 V will occur (duration a few tens of nanoseconds).
I need to consider if any clamping is needed to protect the amplifier.
The datasheet says absolute max differential input voltage 3 V, but it does not say if there is an internal clamp which protects it (provided I limit the current to +/-10 mA) or not.
The post at ... amplifiers/high_speed_amplifiers/f/10/t/624271 [sorry I do not seem to be able to include a hyperlink] by Keyur Tejani (TI) says there is an internal clamp, but that was a side remark off the main topic of that thread. I'd like to really check this statement here. Some amplifiers have internal clamp, some do not, some don't need the input-input clamp. It would be helpful if all opamp datasheets would include a bit more of this info. (Why are the simplified schematic diagrams so much out of favor these days?????)
I understand that as far as clamps to the V+ and V- rails, they are there and the inputs can go to ~0.5V beyond either rail or whatever voltage results in at most 10 mA in those clamp diodes.
I look forward to hearing from you; any advice you can give about clamping and protection in the LMH6629 application will be greatly appreciated.