Other Parts Discussed in Thread: LMH6612
Hi,
I've built a function generator that has the following output stage:
The OPA2830 works without a problem when amplifying sinusoidal signals up to 2MHz. Above that, if the output is terminated with 50 ohms, it starts to show zero-crossing distortion. This distortion worsens with frequency. However, it can be alleviated, and completely eliminated if the signal amplitude is decreased. This shows me that the distortion seems to be slew rate dependent. What confuses me, is that the OPA2830is being used within the specification.
This issue is only caused by the output stage. If the output is left unterminated, or unloaded, it can go well above 4MHz without showing any kind of distortion. What is happening? You can see that there is no distortion at 8MHz, with the amplitude set to 7Vpp and without load.
This is indeed strange.