Hi ,
We are using the PGA 280 in our project , Please address the following queries
>>If we use GPIO4 as an input BUFTin , does the setting of BUF Timeout Register / Register 3 have any effect
>>Do we need to use the buffer trigger 'T'in the upper nibble of the byte of the SPI addressing scheme , if GPIO 4 is used as BUFTin ??
>>Whats is the difference between the bits of register 4 and register 10 , they seem to have the same error flag bits ,Please elucidate
>>How do we use Register 6 & 7 ?
>>Does the BUFPol bit on the Register 10 change the BUFA pin polarity to active high or low ?
>>What is the function of LTD bit /bit 7 on register 11
Regards
Abhay