Hello,
I am evaluating the OPA277 for use in a particular circuit I am designing. For testing purposes, I have constructed a standard non-inverting amplifier with a gain of two, using 100-kOhm resistors in the feedback path and running off +/-15V supplies. I am noticing a large DC output offset voltage (about -20mV) when the input is tied to ground. This is well beyond the spec of the op-amp, even when taking into account all the probable sources of offset, e.g., input bias/offset current, input offset voltage, etc. The offset voltage is also highly sensitive to air currents and also to the value of the the positive supply voltage. When I use the same op-amp in a voltage-follower configuration (with no feedback resistance), the offset voltage is within spec, leading me to believe there might be some excess input bias current flowing into the effective resistance seen at the inverting terminal. Any ideas as to why this might be happening? Thank you.
Matthew