I have a need to drive a low frequency (<1MHz) analog signal over about 6 feet of cable so I am looking for a suitable solution. The parameters that I have been focusing on, and appear to be mutually exclusive and in some cases (Unity Gain Stable) not part of the parameter search.
* Vos (max) < 5mV
* Rail to Rail I/O
* Vs +/- 15v
* High Cap/Current drive
* Unity Gain Stable (Gain will be set to 1:1 or 1.5:1)
The closest that I have come is with the LM8261 or the LM7332, but neither of them list Unity gain stability as a feature.
Suggestions / comments are appreciated.