Hi,
I have setup a test circuit based on Fig.11 of the OPA1632 datasheet, It is actually to drive another type of ADC that requires output common mode of 1.65V. So Vocm was set to 1.65 volts by a ref source and the output bias followed correctly as expected.
However, the inputs now has dc of nearly 1.65V!. So d.c. coupling of signals will be now be affected.
The "virtual earth" points at pin#1 and pin#8 has 1.65V. Was expecting this to be zero under feedback for the inverting amp mode?
Also, if I ground of the inputs for single-ended application, the output common mode gets disturbed and drops to ~1V instead although the ref drive at pin#2 is steady at 1.65V
Thought Vocm affected the outputs only but it seem it affects the input side as well
Please check advise
Thanks