I have the LMP7721 multi-function evaluation board and would like to use it in TIA mode with frequencies in the 1-10 MHz range. Will I run into any issues with either the LMP7721 or the LMP7715 guard driver? It states in page 10 of the users' guide:
"The bandwidth of the guard driver circuit is determined by R1 and C5. The default R1 and C5 values are 10K and 1000pF, which creates a 16 KHz driver bandwidth. For higher bandwidths, these values can be decreased down to 100Ω and 82pF. But some bandwidth limiting should be used to prevent peaking of the buffer at high frequencies, which could cause instability of the entire system."
Should I replace R1 and C5 with 100Ω and 82pF ones since I'm significantly higher than 16 kHz? Just out of curiosity, how are the values of R1 and C5 determined/calculated? All of the voltage follower sites I've read place a direct short between the inverting input and output so I'm not entirely sure how to calculate those values.
Thank you!