Hello, I'm working with the INA826. The documentation on Section 6 (Pin Configuration - Page. 4 shows the pin functionality and position on the 8-pin IC. On Section 11.2 (Layout Example) - Page. 35 it shows an example of laying out the IC and connecting its components. It appears that the layout is inconsistent with the pin positions mentioned in the first section. IE: The layout example diagram shows the same IC, but the pins are in a different position. Which is actually correct? Is this a mistake?