Hello TI,
There appears to be an error with the OPA192 AC analysis.. the AC analysis seems to create a mysterious error at low-frequencies of an additional ~-11 dB?
When operating in transient simulation, there is no loss at these lower frequencies and model operates as expected without the mysterious attenuation...
And if I use a different op-amp it works fine (so its definitely the OP192 model and not my simulation).
TI can you explain?
*Note: Circuit1 has an additional -6dB (1/2 voltage gain) from 50-Ohm matching
*Picture2 transient is working as expected; the buffer shows a circuit gain of -1/2, whereas the inverter has a gain of -1.