HI Experts:
My responsible customer is using the LM231N to convert the voltage to the frequency , there is the frequency tolerance in same batch of boards, means the consistency of frequency is not good . It is around the 10% error . According to the formula below , they checked every component in the formula ,and found the tolerance of the capacitor is 10%.
So can we think the frequency tolerance is caused by the capacitor ? And other factor?