Other Parts Discussed in Thread: INA110, INA116, INA826, INA111, , INA217, INA128
Hello, I am looking for advice for choosing the best amplifier that is to be connected to a Wheatstone Bridge that is supplied with an AC source. I am currently using an INA110 instrumentation amplifier connected to the bridge but it is currently supplied with a DC source. I was wondering if it is possible for this set-up to run the bridge with an AC source? and also, which amplifier would be better, as we are trying to obtain a gain of 10 and run a frequency of 100-300kHz through the amp. Any suggestions are welcomed, thank you!