I am reading a slide document talking about op amp specifications. When it comes to the issue of Vos measurement, a circuit as follow are exhibited. And it was noted that -
"If I was ask to come up with a test circuit for Vos, I would have came up with something like this. When you realize that Vos varies depending on the output, it becomes clear that this circuit is not a good test method."
And it was stated that there are two disadvantages -
"- The finite gain has an effect
- The output isn’t at zero volts (open loop gain error)"
and then, a circuit was provided as follow.
So I just want to ask:
1.How to comprehend that "Vos varies depending on the output "?
2.What will happen if the output isn't at 0 volts for the Vos measurement. Does it has a considerable influence?
3.How the second circuit solve this problem?