Urgently need clarification of the following Electrical Characteristics, Vicm, Viclr, Vichr, found in the datasheet; literal interpretation implies there is dc common mode voltage at each input pin.
Vicm states that is is self-biased to mid-supply (in our case 2.5V DC); Our concern is interference with the DC common mode voltage at the stage driving the LMH6401; are dc blocking capacitors
required in this case ? Is there truly Vicm = 2.5V at each input pin ? Thank you