Hi,
I have questions about AM437x QSPI boot.
The size of flash memory which AM437x QSPI supporting is up to 64MByte.
In Technical Reference Manual(spruhl7g)page.223 "5.2.6.7 QSPI",
it said "support only 24-bit addressable EEPROM".
Q1.Is this means that RBL only support upto 16MByte(24-bit address) QSPI flash?
Q2.If this size(16MByte) is not enough for user application, does user need to make
user boot loader(secondary bootloader) to load the rest of boot image from QSPI to RAM(internal & external)?
best regards,
g.f.