This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
It's May 2018. Is an EVM for PCM3168A available yet?
If not, when do you think it may be available?
Thanks
Hi, Igor,
Unfortunately the EVM for the PCM3168A is not available yet, but we should get it done shortly. In the meantime, could you please share information about your target application?
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hi, Igor,
Two PCM3168s might be used to capture the data of 12 mics, however, please consider that this device is not very flexible and it is not possible for two devices to share the same TDM bus, because there is no way to control the offset of the digital audio. As two audio buses would be required, I think that a better solution would be 3×PCM1864. This device is more flexible and there is an EVM available, as well as the reference design for a circular mic array application.
I am unaware of the files location, I would recommend you to ask with my colleagues of the Processor's forum to find more details about the source files for the project.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer