Other Parts Discussed in Thread: CDCM61001,
Dear support,
I'd like to realize a clock generator to drive the clock input of the DAC3152-EVM. Actually I drive it with a 100MHz clock by a R&S clock generator, and it works fine.
It is possible to use the CDC421A100 ifor the LVPECL output level in single ended mode? Or I must consider the CDCM61001?
I read in fact from the datasheets that the LVPECL outputs are differential for CDC421 and both differential and single ended for CDCM61001.
Do you suggest another components?
Best Regards
Dario