Other Parts Discussed in Thread: LMK04821, LMK04826
Hello Clock Expert,
I'd like to double check that this output frequency setting is workable or not.
CLKin0 : 122.88MHz
External VCXO : 30.72MHz
Using both PLL1 and PLL2
Required Output Frequency : 163.84MHz, 1.92MHz(SYSREF), 245.76MHz, 1966.08MHz, 122.88MHz
It seems like due to bottleneck of VCO1 frequency range, LMK04828 can't generate 1966.08MHz.
Best regards,
Alice