Hello
What is the modulation bandwidth of the LMX2594 by definition?
The Modulation Bandwidth is defined as the maximum rate of change in the output frequency that can be attained using the Control Voltage of a VCXO.
I have seen the response to the other LMX2594 modulation bandwidth post where the "Calibration Free Ramping.pdf" was given. That document describes the maximum and minimum frequency (ramping) that the VCO can be tuned to at a specific lock frequency. Im actually looking for the "maximum rate of change in the output frequency". Most VCXO have this spec listed but I couldnt find it in the datasheet.
Please assist.
Thanks
Layne