Other Parts Discussed in Thread: LMX2592
Hello team,
I have questions about LMX2594 as below. Could you please answer below?
1) 10ms wait time in initial power up sequence programming
Where should we add 10ms wait when Sync mode operation, for example category 2 sync?
Is below sequence correct?
Device power up
Program RESET = 1
Program RESET = 0
Program Reg109
Program Reg108
.....
Program Reg1
Program Reg0 for Sync mode enable
Wait 10ms
Program Reg0 for FCAL_EN
2) PFD control
We can change PFD mode with LMX2592. However in LMX2594, there seems no register for the setting.
In LMX2594 default setting, which PFD mode, Dual or Single is used?
Best regards,