Hi,
I have a few questions about the device from using the LMX2572 Evaluation Board.
1. I seem to have a larger current draw when using the internal channel divider than anticipated
I've tested this on 2 EV boards and seem to get a 20mA current bump (when selecting the CH div) instead of about 10mA in the datasheet
Both boards are clocked externally with a 20MHz Clock and the onboard 100MHz TCXO is disconnected. Charge Pump current is 2.5mA, and the Loop Filter Components give a ~30kHz Bandwidth (changed from the default components that came with the board). Both boards are supplied 3.3V and are configured identically. Output taken from only the positive A channel (B Powered down), negative output terminated 50Ohms.
For the first one:
at 4.5GHz I get 1.23dBm with 67.5mA (vco). at 3GHz I Get 2.2dBm with 87.5mA (div 2)
The second one:
at 4.5GHz I get 1.31dBm with 73.9mA (vco). at 3GHz I Get 2.31dBm with 97.5mA (div 2)
this is about a 20mA bump when the typical current should be about 10mA less with the channel divider on. Is there anything I'm missing about the comfiguration that could warrant the additional current?
+ this is quite a large variance between the cards, and the current specified is only the typical value ~ I was wondering if there is any information for what to expect - max/min current of tested cards etc.
2. In my application I might require to use a 3V regulator instead of the typical 3.3V. If (due to supply voltage accuracy) the voltage were to fall to the 2.9~2.95V range, would there be serious issues with the device's operation? or would you recommend to avoid this scenario at all costs?
How tight of a demand is the voltage requirement?
3. I noticed an issue with the device (oscillation of sorts) when powering down output B, and selecting Output B's source to be High Z
at some frequencies of VCO output A will oscillate/not power on correctly. It usually happened when output A was selected to Channel Divider but it might happen with it selected to VCO too. Changing Output B's source to VCO/Channel Divider fixed this (B is still powered down, didn't matter if it was terminated 50ohm or left open).
I was wondering if this is the reason it is recommended to select VCO for the unused output? or if it is a known issue at all?
Thank you,
Alex