Hi,
For using the LMX2594 as a fixed 10GHz source, only one output - RFoutB, please advise with the following questions:
- Is it right to connect 50 ohm pull-up resistor to each RFoutA outputs?
- For using RFoutB in single ended output mode, is it needed to connect a 50 ohm pull-up resistor to each RFoutB outputs?
- Is it possible to feed the input signal by a single ended 125MHz XO Ref , 6dBm signal level (saturated)? If yes- how is the unused OSCin input terminated ?
thanks