The datasheet states that the SYNC (pin 5), RampCLK (pin 30), RampDir (pin 32) and SysRefReq (pin 28) all be pulled low when not used. Is it safe to directly connect these pins to GND or do should they be pulled down through a resistor? The design is space constrained so we would prefer to connect these inputs directly to ground if possible.
Thank You