Greetings,
I am having trouble getting the CDCE(L)949 programming board to work with either the CDCE913 or the CDCE925. I have tried this on a Windows 7 machine. TI Clock Pro does not see the CDCE(L) 949 programming board (from within TI Clock Pro 1.2, Tools menu->Programming EVM, select correct device from dropdown menu, and click "Find Boards"). Clicking "Find Boards" yields nothing. In the device manager, a "TUSB3410 Device (COM3)" is listed, though it has an exclamation mark. Windows says it cannot verify the digital signature for the drivers installed for this device. I don't know if this is the problem or not.
Thanks,
Tobyn