LMC555 Timer
We have a costumer that is concerned that the data sheet does not explicitly state the minimum operating frequency. Their desire is to operate at 1 HZ. I know this is well within the realm of functionality from experience but this is not clearly stated in the data sheet.
On page 4 of the data sheet, the astable frequency is stated under one test condition and the maximum frequency is also stated, however even in the case of maximum frequency it’s just stated as a typical and therefore of little value, furthermore there is no statement of minimum frequency, as seen below:
Their view is that if it is not specified in the electrical characteristics then it may or may not work at any frequency beyond the minimum and maximum listed.
There is a chart Figure (10) and equations (4) which shows operation at 1HZ. But there is no guarantee that part will work at this speed. How can we justify / guarantee operation if the data sheet does not explicitly state the minimum operating frequency?