I have a question about the ADS 1248 common mode voltage. I have attached a document with calculations showing my understanding of the common mode voltage in my application. I am currently running 300 uA through a 350 ohm resistor and then through a PRT in series and then to ground. I am reading the 350 ohm resistor and the PRT with different analog input channels on the 1248. The noise level is great at low PRT resistances. Once I get up to around 350 ohms on the PRT, which should be full scale, the noise increases dramatically. My question is whether the analog inputs are being exceeded by the 350 ohm resistor. By my calculations the input on the most positive side of the 350 ohm resistor should be 210 mV at full scale which should not be exceeding the common mode voltage at a gain of 16. I have also attached a schematic of my circuit for reference. The circuit is being run in an AC manner by the analog switch on the left side.