Hi , TI engineers, please help me with my problem.
I'm using C6670 AIF2 module, and now most parts are running well, my environment is: CPRI, LTE FDD 20MHZ, 2AxC.
With Tx I'm using 1ms AT event and push 14 symbols into every AxC, it works well.
Rx I'm using PDSP, pdsp will trigger 1 event when it recv 14 symbols, so I should receive 0..13, 14..27, ....., 126..139. every times. and it works fine most times.
But after the system run for a while, the rx side may lost a symbol, the PDSP event will gave me symbol (0..9, 11-14) and the symbol 10 is missing. And then I use the CCS to watch the PDCP ping/pong buf, I can fild the pointers are actually discontinue, which means when the pdsp pop from the AIF2 rx queue, the symbol has already missing.
Thanks for watching my question and hope for you advice.