Hello,
Using IPNC RDK on DM8127 - MT9J003 10Mp sensor.
I need an expert in the TI 2A engine to explain why when the resolution (width) coming from the sensor is less than 3600 wide, the AEC and AWB and SALDRE stop working.
Here's the scenario:
I built a driver with the new resolution based on the default (1920x1080 @ 30fps with binning). The problem is that even though I'm getting the resolution that I want with the correct frame rate, the AGC/AWB and SALDRE have stopped working.
We need a frame resolution of 1200x1200 @ 20fps (binning from 2400x2400) from the center of the sensor.
When I made the changes gradually, I found that 1800x1200 (binning from 3600x2400) still gives me the correct AGC, AWB and SALDRE.
Once I go down to 1600x1200 (3200x2400), I lose all of the "automatic" frame processing functions - the AGC/AWB and SALDRE have stopped working.
I'd appreciate any help you can offer,
Thanks,
Mechi