Hi,
Can TMS320DM8165 support external Sync mode for 16bit/24bit YCbCr/RGB video channel input?
Thanks.
Regars,
Alpesh
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can TMS320DM8165 support external Sync mode for 16bit/24bit YCbCr/RGB video channel input?
Thanks.
Regars,
Alpesh
Hello,
I would recommend you to check the TRM :
High-Definition Video Processing Subsystem (HDVPSS)
BR
Margarita
Hi Margarita,
Thanks for your support.
In section 2.11 Video Input Parser (VIP) Module and its provide information of YUV format but we need information of RGB and YCbCR interface.please correct me if i miss understanding.
We need to interface ADV7612 HDMI receiver with TMS320DM8168 processor.
Can you please help me for how to interface ADV7612 HDMI receiver with HDVPSS of TMS320DM8168?
Thanks.
Regards,
Alpesh
Hi Alpesh,
Vip supports external Sync mode for 16bit/24bit YCbCr/RGB.
Regards,
Brijesh
Hi Brijesh,
Thanks for your support
Yes, It is provide digital parallel port output.
Please see attached image for more information.
I have confusion for interface how to interface ADV7612 with DM8168 processor and it should work or not.I am work on first time for this type application.
Thanks
Regards,
Alpesh
Hi Alpesh,
They both are same, as long as, it can output YUV/YCbCr output on digital parallel interface, VIP will be able to capture it..
Regards,
Brijesh