Hi,
I'm working on LCDK6748 with TIRTOS v. 2.0.1.23 , XDC 3.30.3.47 and CCS v6.0.1.00040. Codec is AIC3106 and DSP is OMAPL138. I wrote a simple program to perform Audio Echo chanel sample by sample. I'm generating sine wave with 400Hz and amplitude 390mV. My code alows me to acquire sine wave :
,but returned signal is heavily distorted :
I have no idea what is the issue of this distortion. Is anybody have any clue what am I doing wrong? Below I attach file with my init codes for McAsp, codec and with main().
Thanks,
Best Regards
Mirek
int main(void) { /*PinMuxSetup for all peripherals*/ I2CPinMuxSetup(0); McASPPinMuxSetup(); /*PowerUp modules */ PSCModuleControl(SOC_PSC_1_REGS, HW_PSC_MCASP0, PSC_POWERDOMAIN_ALWAYS_ON, PSC_MDCTL_NEXT_ENABLE); BIOS_start(); } void runningThread(void) { /* i2c init */ I2CCodecIfInit(SOC_I2C_0_REGS ,INT_CHANNEL_I2C , I2C_SLAVE_CODEC_AIC31); /* codec configuration */ codecInit(); /* mcasp configuration */ McASPConfigure(); while(1) { /* loop */ } } /* McAsp ISR */ void McASP_ISR(void) { Sample = McASPRxBufRead(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_RX); Swi_post(AudioSWI); } /* SWI */ void AudioProcessSWI(void) { static UInt j =0,k =0; /* Data from left channel */ if(HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RSLOT)) { Buffer[j]=(Int16)Sample; //Sample = Buffer[j]; j+=1; j= j%256; } else { Buffer2[k]=(Int16)Sample; k+=1; k= k%256; Sample = 0 ; } while(!(HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XSTAT)&0x20)); /* wait untill empty */ McASPTxBufWrite(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_TX,Sample);//(Int)sinetable[i]); while((HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XSTAT)&0x20)); /* wait untill full */ } /* AIC3106 configuration: */ /* Set the sample Rate */ CodecRegWrite(baseAddr, AIC31_P0_REG2, 0x00); CodecRegWrite(baseAddr, AIC31_P0_REG3, 0x22); /* use PLL_CLK_IN as MCLK */ CodecRegWrite(baseAddr, AIC31_P0_REG102, 0x00); /* Use PLL DIV OUT as codec CLK IN */ CodecRegBitClr(baseAddr, AIC31_P0_REG101, 0x01); /* Select GPIO to output the divided PLL IN */ //CodecRegWrite(baseAddr, AIC31_P0_REG98, 0x20); CodecRegWrite(baseAddr, AIC31_P0_REG4, 0x40); /* Configure the PLL divide registers */ CodecRegWrite(baseAddr, AIC31_P0_REG5, 0x6D); CodecRegWrite(baseAddr, AIC31_P0_REG6, 0x60); CodecRegWrite(baseAddr, AIC31_P0_REG11, 0x01); /* Enable the codec to be master for fs and bclk */ CodecRegWrite(baseAddr, AIC31_P0_REG8, 0x00); /* Slave Mode */ //CodecRegWrite(baseAddr, AIC31_P0_REG8, 0xD0); /* Master Mode */ CodecRegWrite(baseAddr, AIC31_P0_REG7, 0x0A); /* Write the data type and slot width */ CodecRegWrite(baseAddr, AIC31_P0_REG9, 0x06); /* valid data after dataOff number of clock cycles */ CodecRegWrite(baseAddr, AIC31_P0_REG10, 0x00); /* ADC Mono */ /* enable the programmable PGA for left and right ADC */ CodecRegWrite(baseAddr, AIC31_P0_REG15, 0x00); CodecRegWrite(baseAddr, AIC31_P0_REG16, 0x80); /* Right ADC is muted */ /* power off the Line L1L */ CodecRegWrite(baseAddr, AIC31_P0_REG19, 0x04); /* power on the Line LIR */ CodecRegWrite(baseAddr, AIC31_P0_REG22, 0x00); /* power up the left and right(off) DACs */ CodecRegWrite(baseAddr, AIC31_P0_REG37, 0xA0); /* select the DAC L1 R1 Paths */ CodecRegWrite(baseAddr, AIC31_P0_REG41, 0x00); /* Mono settings */ CodecRegWrite(baseAddr, AIC31_P0_REG42, 0x6C); /* Driver power-on time/ ramp-up step time*/ /* DAC L to HPLOUT Is NOT connected */ CodecRegWrite(baseAddr, AIC31_P0_REG47, 0x7F); CodecRegWrite(baseAddr, AIC31_P0_REG51, 0x7F);/* is off*/ /* DAC R to HPROUT is NOT connected */ CodecRegWrite(baseAddr, AIC31_P0_REG64, 0x7F); CodecRegWrite(baseAddr, AIC31_P0_REG65, 0x7F); /* is off */ /* DACL1 connected to LINE1 LOUT */ CodecRegWrite(baseAddr, AIC31_P0_REG82, 0x80); /* DAC_L1 is connected */ CodecRegWrite(baseAddr, AIC31_P0_REG86, 0x09); /* unmuted/power on */ /* DACR1 connected to LINE1 ROUT */ CodecRegWrite(baseAddr, AIC31_P0_REG92, 0x00); /* DAC_R1 is not connected */ CodecRegWrite(baseAddr, AIC31_P0_REG93, 0x00); /* muted/power off */ /* unmute the DAC */ CodecRegWrite(baseAddr, AIC31_P0_REG43, 0x00);/* left channel is mute */ CodecRegWrite(baseAddr, AIC31_P0_REG44, 0x80); /* McASP configuration: */ /* reset MCasp (GBLCTL) */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RGBLCTL)= 0; HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XGBLCTL) = 0; /* Receiver configuration */ /* Configure Mask */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RMASK) = 0x0000FFFF; /* Configure format of receive section */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RFMT) = 0x0001807C; /* 1 bit delay/MSB/slot size 16bit/read from Periph */ /* Clocks control */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_AFSRCTL) = 0x00000112; /* I2S mode/ internal frame clock/ rising edge */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_ACLKRCTL) = 0x000000AF; /* rising edge/ Divide by 16 */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_AHCLKRCTL) = 0x00000000; /* Divide by 1/ clock source from AUCLKX */ /* Set Active Slots */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RTDM) = 0x00000003; /* Configure receiver clock check circuit */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RCLKCHK) = 0x00FF0008; /* Transmitter configuration */ /* Configure Mask */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XMASK) = 0x0000FFFF; /* Configure format of transmitt section */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XFMT) = 0x0001807C; /* 1 bit delay/MSB/slot size 16bit/read from Periph */ /* Clocks control */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_AFSXCTL) = 0x00000112; /* I2S mode/ internal frame clock/ rising edge */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_ACLKXCTL) = 0x000000AF; HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_AHCLKXCTL) = 0x00000000; /* Set Active Slots */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XTDM) = 0x00000003; /* Configure transmitter clock check circuit */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XCLKCHK) = 0x00FF0008; /* Set serializers numbers */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_SRCTL(13u)) = 0x0000000D; /* Set serializer13 as transmitter */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_SRCTL(14u)) = 0x0000000E; /* Set serializer13 as receiver */ /* Configure pins */ /* Set McASP as GPIO */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_PFUNC) = 0; /* Set Pins Direction */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_PDIR) = 0x14002000; /* Enable DIT mode transmission */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_DITCTL) = 0x00000000; /* Enable DLB mode transmission */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_DLBCTL) = 0x00000000; /* Configure McAsp Mute */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_AMUTE) = 0x00000000; /* if clk clock failed set mute */ /* Start McAsp : */ /* Transmit high-frequency clock divider is running */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XGBLCTL) |= 0x00000200; /* XHCLKRST */ /* Wait untill it's working */ while(!(HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XGBLCTL)&(0x00000200))); /* Receive high-frequency clock divider is running */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RGBLCTL) |= 0x00000002; /* RHCLKRST */ /* Wait untill it's working */ while(!(HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RGBLCTL)&(0x00000002))); /* Transmit clock divider is running*/ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XGBLCTL) |= 0x00000100; /* XCLKRST */ /* Wait untill it's working */ while(!(HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XGBLCTL)&&0x00000100)); /* Receive clock divider is running*/ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RGBLCTL) |= 0x00000001; /* RCLKRST */ /* Wait untill it's working */ while(!(HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RGBLCTL)&&0x00000001)); /* Set Interrupts */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RINTCTL) = 0x00000020; /* Data ready Interrupt */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XINTCTL) = 0x00000020; /* Transmit Data ready/ Sync Frame Start Interrupts */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RSTAT) = 0x0000FFFF; /* Clear Receiver Status Register */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XSTAT) = 0x0000FFFF; /* Clear Transmitter Status Register */ /* Transmit serializers are active */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XGBLCTL) |= 0x00000400; /* XSRLCR */ /* Wait untill it's working */ while(!(HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XGBLCTL)&(0x00000400))); /* Receive serializers are active */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RGBLCTL) |= 0x00000004; /* RSRLCR */ /* Wait untill it's working */ while(!(HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RGBLCTL)&(0x00000004))); /* Send 0, so that no underrun occurs after releasing the staet machine */ McASPTxBufWrite(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_TX, 0); /* Transmit state machine is released from reset */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XGBLCTL) |= 0x00000800; /* XSMRST */ /* Wait untill it's working */ while(!(HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XGBLCTL)&(0x00000800))); /* Receive state machine is released from reset */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RGBLCTL) |= 0x00000008; /* RSMRST */ /* Wait untill it's working */ while(!(HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RGBLCTL)&(0x00000008))); /* Transmit frame sync generator is active */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XGBLCTL) |= 0x00001000; /* XFRST */ /* Wait untill it's working */ while(!(HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XGBLCTL)&(0x00001000))); /* Receive frame sync generator is active */ HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RGBLCTL) |= 0x00000010; /* RFRST */ /* Wait untill it's working */ while(!(HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_RGBLCTL)&(0x00000010))); while(!(HWREG(SOC_MCASP_0_CTRL_REGS + MCASP_XSTAT)&0x20)); McASPTxBufWrite(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_TX, 0);