The datasheet for the OMAP-L137 (page 61) states that for input clock frequencies between 20 and 30 MHz, a crystal with 60 ohm max ESR is recommended and typical load capacitance values are 10-20 pF. I have been searching for a crystal with a 4-SMD (2.5mm x 2.00mm) package to replace the original crystal that is now obsolete in my design. This is the crystal that I found that comes closest to meeting the OMAP-L137 requirements:
MFG PN: NX2520SA-24.576000MHZ
MFG: NDK America, Inc.
It has a Load Capacitance of 10 pF (Requirement is 10-20pF)
However, it has an ESR of 70 ohm (Requirement per the datasheet is 60 Ohm max). Will this be a problem?
Thanks