Hi,
I am trying to modify the AM335X Starter Kit to be able to work with a 7" LCD.
I have two screens that I am working with:
***TFC-A9700RTWV35TR-02A (from FiveThreeCorp), this is the primary screen I would like to get working.
4D 7.0" LCD Cape (from 4D systems)
I am aware that the LCD driver IC can be re-configured to allow for higher voltage/current.
The primary screen has the same VDD voltage as the NHD-4.3-480272MF-ATXI-T-1 (screen that comes with the AM335x starter kit) which is 3.3V.
The main differences are dealing with the back light current and voltage. (22-23V @ 40mA max vs. 22-24V @ 60mA max). The later being the TFC screen.
My question is: with using the Android OS that came with this kit, does the image need to be re-compiled to enable the correct driver to be used with a 7" screen?
Or should the screens be directly interchangeable with the exception of the mods needed for the LCD driver IC?