Hey,
Bios 6.4 TiRTOS 2.02.36 CCS6
1. Main:
// ....Set FPU FPULazyStackingEnable(); FPUEnable(); /* *** *** START BIOSU *** *** */ //System_printf("exit main()\n"); //Breakpoint One BIOS_start(); /* does not return */ return(0); }
2. FPCC = 0xC0000000
3. The problem is that after BIOS start, FPCC=0x0000000 .And FPU does not work properly - sometimes are calculating errors.
4. When i add lines AFTER BIOS started:
FPUEnable();
FPULazyStackingEnable();
FPU works properly and calculations are good.
So question: Is is normal that BIOS clear fpu config? Can i call FPULazyStackingEnable() after bios started?