This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CONVERT LVDS SIGNAL TO CSI-2

Intellectual 365 points

Replies: 13

Views: 5348

Hi all,

Anyone have an idea about LVDS convert to CSI-2  help me pls?. I don't have an idea about it yet.

Thank you all,

  • In reply to Darryl Jeong:

    Also, yes these devices will support 1080p
  • In reply to Darryl Jeong:

    Hi Jeong,

    Thank you for your 's help.

    My question are:

    1. I use 2 lane data LVDS + 1 lane clock input DS90UH947-Q1, output 1 or 2 lane FPD Link III?. Can DS90UH947-Q1 in this case can support 1920x1080p 60 frame per seconds?.

    2. I know DS90UH947 auto detect DS90UH940, so if i only use 1 lane PFD Link III input DS90UH940, DS90UH940 output 1 or 2 lane CSI-2?. How many max bit rate DS90UH940 can transfer?. 

    For more details, I use camera Hitachi DI -SC233. Signal output is LVDS. I only use 2 lane LVDS data + 1 lane clock.

    Looking forward you respone soon.

    Best regards,

    Bang

  • In reply to Darryl Jeong:

    Hi,
    I want design module convert LVDS signal to MIPI CSI-2, so i decide to use LVDS -> DS90UB947-Q1 -> DS90UB940-Q1. I read datasheet said need STP or Coaxial cable connect between DS90UB947 and DS90B940. Can I only use track connect DOUT+/DOUT- from DS90UB947 to RIN+/RIN- DS90UB940 in same PCB? If I can, how many impedance suitable for this case?. If not, can you help me an idea about STP or coaxial cable connect between DS90UB947 and DS90UB940?.
    Best regards,
    Bang Duong

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.