This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD1792: Current limit in case of short to GND of A/B pin

Part Number: SN65HVD1792

Dear all,

is there any protection to limit the current in case of short of A or B pin to GND ?

Will be there only a thermal shutdown ?

regards,

Domenico

  • Hi Domenico,

    In addition to the thermal shutdown, SN65HVD1792 also features short-circuit current limiting of the driver outputs. This ensures that the maximum current flowing into or out of the RS-485 bus is 250 mA (see the "IOS" specification).

    Please let me know if you have any additional questions.

    Regards,
    Max