This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TFP401: Problem interfacing TFP401 to DLPC3439

Intellectual 440 points

Replies: 4

Views: 143

Part Number: TFP401

Hello!

I have designed my own PCB which is based on DLPDLCR4710EVM.

Instead of ITE6801, I used a TFP401 as a HDMI decoder not including voice.

The source of HDMI is output of desktop computer video card.

And the resolution of HDMI is  a full HD of 1920 x 1080.

I have a problem interfacing the TFP401 to DLPC3439.

As the attached image, the displayed image is not good.

The half of image is normal and the other is abnormal.

I have posted about this problem as like the below link.

https://e2e.ti.com/support/dlp/f/94/t/741486

The conclusion of this post is that there is no problem interfacing DLPC3439 to DLP4710.

But I have no confidence between TFP401 and DLPC3439

According to the TFP401 datasheet, it shows that the TFP401 supply WUXGA resolution.

What I want to know is that the TFP401 is a proper decoder for interfacing with the DLPC3439 in  full HD mode.

I'd like to approach this problem in a view of TFP401.

Please, help me to solve this problem.

Thanks!

Regards

Yun-Seok Cho

  • Hi Yun-Seok,

    Have you checked the pin-mapping between the TFP401 and DLPC3439? Can you share your schematic with me at i-anyiam@ti.com?

    Regards,
    I.K.
  • In reply to I.K. Anyiam:

    Hi Anyiam,

    Yes. I have checked the pin-mapping between TFP401 and DLPC3439.

    But I couldn't find out any problem.

    On my own board, I'm using two of DLPC3439.

    The master and slave of DLPC3439 are sharing the same signals from TFP401.

    The signals are like below.

    1. Data : 24bit

    2. HYSNC, VSYNC, ODCK, DEN

    Am I right?

    I sent the schematic by your e-mail.

    Thank you for your time!

    Regards

    Yun-Seok Cho

  • In reply to Yun-Seok Cho:

    Hi Yun-Seok,

    The pin mapping looks okay. Other than that the issue may be with HSYNC/VSYNC on one half of the image. From the schematic it looks like the TFP401 is driving 2x DLPC3439, so one of them is likely not getting the correct timing. This would not be an issue with the TFP401, however, as it is just passing the signals through. I recommend investigating HSYNC/VSYNC for irregularities.

    Regards,
    I.K.
  • In reply to I.K. Anyiam:

    Hi Anyiam,

    Thanks for your answer.

    As you recommend me, I'll try to investigate the signal of HSYNC/VSYNC.

    Regards

    Yun-Seok Cho

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.