Hi team,
I am considering the application of TFP401 or TFP401A.
To display HDMI output of PI compute module 3+ on TFT-LCD through RGB digital input.
I try to make a conversion circuit using TFP401.
In this case, do you need an HDMI license to purchase and use the TFP401?
In addition, there is no connector outside the product, and the signal is not output. Also, we don’t use the audio and use the video only.
Connect the HDMI output of BCM2837B0 on raspberry PI compute module 3+ directly to the TFP401 on the board we make without using the HDMI connector.
Best Regards,
Tom Liu