I need information of IOH-VOH and IOL-VOL characteristic curve of SN75ALS191.
Datesheet has VOH(or VOL)values of IOH=-10mA and -40mA(or 40mA).
However, customer needs VOH(or VOL)values of IOH=-5mA(or 5mA).
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need information of IOH-VOH and IOL-VOL characteristic curve of SN75ALS191.
Datesheet has VOH(or VOL)values of IOH=-10mA and -40mA(or 40mA).
However, customer needs VOH(or VOL)values of IOH=-5mA(or 5mA).
Hi, Roland-san
Its reason is that customer don't want to change their circuit.
Because their module has correct behavior.
However, they found the issue that the calculated value has out of behavior range.
They thinks that circuit has correct in IC's real ability.
Best Regards,
Mitsuo Hirata
Mitsuo-san,
I recorded VOH and VOL from 0mA to 40mA.
I used three VCC [4.5V, 5V, 5.5V] and four temperatures [0C, 25C, 70C, 125C]
I still don't understand why the data is needed.
I was surprised to see 0 mA VOL wasn't closer to zero.
Hi,Michalick-san
Thank you for your answer and the recorded data.
Customer will have satisfaction.
>I still don't understand why the data is needed.
I have only informaiton above.
I requested to sales to get information of reason.
When I receive it, I will answer you.
Thank you very much, again.
Best regards,
Mitsuo Hirata