Hi,
I have a question about SN65HVD33 RS-485 Tranceiver.
The maximum data rate of SN65HVD33 is 26Mbps.
I understood that data rate will depend to bus length.
If bus length are long that the data rate will be slower.
I want to know whether the data rate will also depend to the number of connected node.
Q1.
Does the data rate vary depending on the number of connected nodes?
Q2.
We are planning to connect 32 nodes to the bus.
In this case, is it possible to communicate at a maximum of 26 Mbps?
Or will it be much less than 26Mbps, for example about half data rate of 26Mbps?
best regards,
g.f.