This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MAX3223: Can we connect 2 UARTs of a processor to MAX3223 ?

Part Number: MAX3223

Hi I am using MAX3223 device in my design. And I have 2 PHYTEC processors in my overall system [ 2 mother boards].

I need to have 2 separate UART/RS232 connectors for getting system logs, one per PHYTEC.

So i need to have UART to RS232 line drivers in my design.

Since MAX3223 is a dual channel line driver can i connect 2 separate UART ports to MAX3223 device and take 2 separate RS232 signals and provide to RS232 connector?

With the RTS and CTS in picture (with flow control in picture) only one fully functional UART/RS232 translation can be achieved with MAX3223 device and since I am not using RTS and CTS, I am thinking to use 2 separate UARTS with MAX3223 chip. Need advise on this.

refer to attached picture for my application details.