please help me to get footprint details (pad size, solder mask and paste mask) of part SN74AVC16834
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
please help me to get footprint details (pad size, solder mask and paste mask) of part SN74AVC16834
Hi Shreyas,
Details given datasheet is only for package, there is no details of footprint.
I need footprint related details as similar that is given in document DGG0056A. See attached document.
I use DGV package type (TVSOP) 56-pin in design .
Br / NarendraFootprint Refrence TSSOP-56.pdf
Hi Shreyash,
Thank you very much for sharing the document. Yes it answers my queries.
But I have a doubt about pad size (0.2mm) which is smaller in width as compared to maximum size of pin width (0.23mm)
Is that OK?
Also, why there are two methods of solder mask? In which situation other method "SOLDER MASK DEFINED" is used? Please, provide information in detail.
Br / Narendra