Hello,
Regarding to output on SN74AUP1G17, my customer is asking a question.
(Question)
When their conditions are as following, how does output level become?
(High or low or unknown?)
・Vcc<0.8V (under 0.8V)
・Input A =2.55V-3.4V
Basically, I think that the device is not damaged at input 3.4V, because of Absolute Maximum Ratings.
But I’m not sure how output level become on above conditions.
Regards,
Tao_2199