Hi,
I'm interfacing MSP430F5529 launchpad with ADS1248 via SPI. I was monitoring the UCB0TXBUF and RXBUF registers while running CCS and found that only TXBUF is getting the values and RXBUF always return 0x00 whenever a register is read. I first want to have a setup where I can write and read back registers properly. Upon seeing the waveforms of SPI on DSO, I found that the SCLK gets turned off whenever RXBUF is being used to read data. Please help in solving this issue. Please find the attachments of code and the waveforms below.
#include <msp430.h> #include "ADS_settings.h" void config_CLOCK(void); //8MHz void CONFIG_SPI_ADS(void); //UCB0 as SPI unsigned char REG_ADDR[15] = {MUX0,VBIAS,MUX1,SYS0,OFC0,OFC1,OFC2,FSC0,FSC1,FSC2,IDAC0,IDAC1,GPIOCFG,GPIOCDIR,GPIODAT}; unsigned char REG_VAL[15]= {MUX0_VAL,VBIAS_VAL,MUX1_VAL,SYS0_VAL,OFC0_VAL,OFC1_VAL,OFC2_VAL,FSC0_VAL,FSC1_VAL,FSC2_VAL,IDAC0_VAL,IDAC1_VAL,GPIOCFG_VAL,GPIOCDIR_VAL,GPIODAT_VAL}; unsigned char READ_REG[15]={0x00}; unsigned char read_data = 0; unsigned char dummy = 0; int main(void) { WDTCTL = WDTPW | WDTHOLD; // Stop watchdog timer config_CLOCK(); CONFIG_SPI_ADS(); //__bis_SR_register(GIE); //enable interrupts __delay_cycles(10000); P2OUT &= ~ BIT5; //RESET pin low - resets digital circuits __delay_cycles(100000); P2OUT |= BIT5; //RESET high P2OUT |= BIT6; //CS high P2OUT |= BIT4; //Make START pin as HIGH while(1) { P2OUT &= ~BIT6; //Make CS low while (!(UCB0IFG & UCTXIFG)); // Make sure nothing is already in the TX buffer UCB0TXBUF = 0x40; // Send the write commmand with 0x00 as start address while (!(UCB0IFG & UCRXIFG)); // Before returning wait until transmission is complete dummy = UCB0RXBUF; while (!(UCB0IFG & UCTXIFG)); // Make sure nothing is already in the TX buffer UCB0TXBUF = 0x00; // Send the no. of registers to be written while (!(UCB0IFG & UCRXIFG)); // Before returning wait until transmission is complete dummy = UCB0RXBUF; while (!(UCB0IFG & UCTXIFG)); // Make sure nothing is already in the TX buffer UCB0TXBUF = 0x01; // Send the register value while (!(UCB0IFG & UCRXIFG)); // Before returning wait until transmission is complete dummy = UCB0RXBUF; while (!(UCB0IFG & UCTXIFG)); // Make sure nothing is already in the TX buffer UCB0TXBUF = 0x20; // Send the read register command while (!(UCB0IFG & UCRXIFG)); // Before returning wait until transmission is complete UCB0IFG &= ~(UCRXIFG); dummy = UCB0RXBUF; while (!(UCB0IFG & UCTXIFG)); // Make sure nothing is already in the TX buffer UCB0TXBUF = 0x00; // Send the no.of registers to read while (!(UCB0IFG & UCRXIFG)); // Before returning wait until transmission is complete dummy = UCB0RXBUF; while (!(UCB0IFG & UCTXIFG)); // Make sure nothing is already in the TX buffer UCB0TXBUF = 0xFF; // Send dummy Byte to take data from register while (!(UCB0IFG & UCRXIFG)); // Before returning wait until transmission is complete read_data = UCB0RXBUF; //store the register value P2OUT |= BIT6; //Make CS high __delay_cycles(10000); } } void config_CLOCK(void) //SMCLK CONFIGURAATION { volatile unsigned int i; P1DIR |= BIT1; // P1.1 output P1DIR |= BIT0; // ACLK set out to pins P1SEL |= BIT0; P2DIR |= BIT2; // SMCLK set out to pins P2SEL |= BIT2; P7DIR |= BIT7; // MCLK set out to pins P7SEL |= BIT7; UCSCTL3 = SELREF_2; // Set DCO FLL reference = REFO UCSCTL4 |= SELA_2; // Set ACLK = REFO UCSCTL0 = 0x0000; // Set lowest possible DCOx, MODx // Loop until XT1,XT2 & DCO stabilizes - In this case only DCO has to stabilize do { UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG); // Clear XT2,XT1,DCO fault flags SFRIFG1 &= ~OFIFG; // Clear fault flags }while (SFRIFG1&OFIFG); // Test oscillator fault flag __bis_SR_register(SCG0); // Disable the FLL control loop UCSCTL1 = DCORSEL_5; // Select DCO range 16MHz operation UCSCTL2 |= 15; // (N + 1) * FLLRef = Fdco __bic_SR_register(SCG0); // Enable the FLL control loop // Worst-case settling time for the DCO when the DCO range bits have been // changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx // UG for optimization. // 32 x 32 x 8 MHz / 32,768 Hz = 250000 = MCLK cycles for DCO to settle __delay_cycles(250000); } void CONFIG_SPI_ADS(void) //SPI initialization { UCB0CTL1 |= UCSWRST; //set software reset to 1 so we can configure SPI //UCB0STAT |= UCLISTEN; //the launchpad listens to itself (use for testing) UCB0CTL0 |= UCCKPH+UCMSB + UCMST + UCSYNC; //clkphase,clkpolarity,MSBfirst,8-bit,master mode, 3-pin, synchronous SPI UCB0CTL1 |= UCSSEL_2; //choose SMCLK as our clock. SMCLK is 1.1 MHz. We divise it with the baud register UCB0BR0 |= 0x02; //Prescalar for the SCLK (2 bytes). Here it sets 8MHz sclk to 4MHz UCB0BR1 = 0; //upper byte of br register. set to zero __delay_cycles(10); P1DIR &= ~BIT1; //DRDY - Input to MCU P2DIR |= BIT4; //START - Output from MCU P2DIR |= BIT5; //RESET - Output from MCU P2DIR |= BIT6; //CS - Output from MCU P3DIR |= BIT0+BIT2; //3.0-MOSI, 3.2-SCLK Output from MCU P3DIR &= ~BIT1; //3.1 MISO Input to MCU P3SEL |= (BIT0 | BIT1 | BIT2); //configures pins for three pin SPI. MISO P3.1, MOSI P3.0, SCLK P3.2 __delay_cycles(10); UCB0CTL1 &= ~UCSWRST; //enables the SPI to work UCB0IE |= UCTXIE+UCRXIE; // Enable USCI0 TX AND RX interrupt }
SCLK (2) - CS (1) SIGNALS:
SCLK (2) - MOSI (1) SIGNALS:
SCLK (2)- MISO (1) SIGNALS:
Please let me know if further information is required.
Thanks & Regards,
Vignesh