Tool/software: Code Composer Studio
Hi,
so i have this code which from the times i executed it seems to do what i entended for it to do from the first place: ''entering Hibernate mode and then waking up with external push button''.
i'm suppose to make sure that my board did actualy enter hibernate mode and then woke up.
//***************************************************************************** // // The error routine that is called if the driver library encounters an error. // //***************************************************************************** #ifdef DEBUG void __error__(char *pcFilename, uint32_t ui32Line) { } #endif //***************************************************************************** // // Configure the UART and its pins. This must be called before UARTprintf(). // //***************************************************************************** void ConfigureUART(void) { // // Enable the GPIO Peripheral used by the UART. // ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); // // Enable UART0 // ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0); // // Configure GPIO Pins for UART mode. // ROM_GPIOPinConfigure(GPIO_PA0_U0RX); ROM_GPIOPinConfigure(GPIO_PA1_U0TX); ROM_GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1); // // Use the internal 16MHz oscillator as the UART clock source. // UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC); // // Initialize the UART for console I/O. // UARTStdioConfig(0, 115200, 16000000); } //***************************************************************************** // // The interrupt handler for the Buttons. // //***************************************************************************** void BottonsHandler(void){ if((GPIOIntStatus(GPIO_PORTF_BASE,true)& Buttoninit1)) { GPIOIntClear(GPIO_PORTF_BASE,Buttoninit1);// Clear interrupt flag TimerEnable(TIMER0_BASE, TIMER_A);//Enables the timer } else if((GPIOIntStatus(GPIO_PORTF_BASE,true)& Buttoninit0)) { GPIOIntClear(GPIO_PORTF_BASE,Buttoninit0);// Clear interrupt flag TimerDisable(TIMER0_BASE, TIMER_A);//Disables the timer SysCtlPeripheralDisable(SYSCTL_PERIPH_HIBERNATE);//Disables the Hibernation module HibernateGPIORetentionDisable();//Disable GPIO retention HibernateDisable();//Disables the Hibernation module for operation. } } void configureButtons(void){ //configureButton0 GPIOPinTypeGPIOInput(ButtonBase, Button0); GPIOPadConfigSet(ButtonBase ,Button0,GPIO_STRENGTH_2MA,GPIO_PIN_TYPE_STD_WPU);// Register our handler function for port F GPIOIntTypeSet(GPIO_PORTF_BASE,GPIO_PIN_0,GPIO_FALLING_EDGE);// Configure PF4 for falling edge trigger GPIOIntRegister(GPIO_PORTF_BASE,BottonsHandler); // Register our handler function for port F GPIOIntEnable(GPIO_PORTF_BASE, GPIO_INT_PIN_0);// Enable interrupt for PF0 //configureButton1 GPIOPinTypeGPIOInput(ButtonBase, Button1); GPIOPadConfigSet(ButtonBase ,Button1,GPIO_STRENGTH_2MA,GPIO_PIN_TYPE_STD_WPU);// Register our handler function for port F GPIOIntTypeSet(GPIO_PORTF_BASE,GPIO_PIN_4,GPIO_FALLING_EDGE);// Configure PF4 for falling edge trigger GPIOIntRegister(GPIO_PORTF_BASE,BottonsHandler);// Register our handler function for port F GPIOIntEnable(GPIO_PORTF_BASE, GPIO_INT_PIN_4);// Enable interrupt for PF4 } void Timer0IntHandler(void) { // // Clear the timer interrupt. // TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT); UARTprintf("Hibernate mode is on!\n"); SysCtlPeripheralEnable(SYSCTL_PERIPH_HIBERNATE);// enable the hibernation module HibernateEnableExpClk(SysCtlClockGet());//defines the clock supplied to the hibernation module HibernateGPIORetentionEnable(); //Calling this function enables the GPIO pin state to be maintained during hibernation . SysCtlDelay(SysCtlClockGet()/10 ); HibernateWakeSet(HIBERNATE_WAKE_PIN);//set the wake condition to the wake pin SysCtlDelay(SysCtlClockGet()/10 ); GPIOPinWrite(GPIO_PORTF_BASE,GPIO_PIN_3, 0);//turn off the green LED before the device goes to sleep. /*enable the device to wake on either the RTC or the WAKE pin. */ //HibernateRTCSet(0); //HibernateRTCEnable(); // HibernateRTCMatchSet(0,10); //HibernateWakeSet(HIBERNATE_WAKE_PIN | HIBERNATE_WAKE_RTC); /*function requests the Hibernation module to disable the external regulator, removing power from the processor and all peripherals.*/ HibernateRequest(); } //***************************************************************************** // // Print "Hello World!" to the UART on the evaluation board. // //***************************************************************************** int main(void) { //volatile uint32_t ui32Loop; // // Enable lazy stacking for interrupt handlers. This allows floating-point // instructions to be used within interrupt handlers, but at the expense of // extra stack usage. // //ROM_FPULazyStackingEnable(); // // Set the clocking to run directly from the crystal. // ROM_SysCtlClockSet(SYSCTL_SYSDIV_5 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ | SYSCTL_OSC_MAIN); // // Enable the GPIO port that is used for the on-board LED. // ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF); // // Enable the GPIO pins for the LED (PF2 & PF3). // ROM_GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3); // // Enable the peripherals used by this example. // ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0); // // Enable processor interrupts. // ROM_IntMasterEnable(); // // Configure the two 32-bit periodic timers. // ROM_TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC); ROM_TimerLoadSet(TIMER0_BASE, TIMER_A, ROM_SysCtlClockGet()); // // Setup the interrupts for the timer timeouts. // ROM_IntEnable(INT_TIMER0A); ROM_TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT); // // Registers an interrupt handler for the timer interrupt. // TimerIntRegister(TIMER0_BASE,TIMER_A,Timer0IntHandler); // // Initialize the UART. // ConfigureUART(); // //Initialize the Buttons. // configureButtons(); // // Hello! // UARTprintf("Hello, world!\n"); SysCtlDelay(SysCtlClockGet()); while(1) { UARTprintf("Run mode is on!\n"); SysCtlDelay(SysCtlClockGet()); GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3,GPIO_PIN_3 ); SysCtlDelay(SysCtlClockGet()/10 ); GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_3,0); SysCtlDelay(SysCtlClockGet()/10 ); } }
i don't know how to proceed...any help !!
regards
amine