Other Parts Discussed in Thread: USB2ANY, DRV10983, DRV10987
Hello,
I too am having an issue I can't get around regarding a write error:
DRV10983 USB2ANY.lvclass:Write
Register.vi<ERR>
Register writing not successful!!!
I do have the 3 voltages present and correct. I tried to reboot many times. Tried different power up sequencing. I have 15V from power supply (tried 12V as well).
I did an install using the default directories created by the installer. I am using Win 10. Is that the issue?
Thanks,
Russ