Other Parts Discussed in Thread: TMS570LS1224, BQ76PL455A-Q1, HALCOGEN
Hi, I am developing a battery management system for an electric vehicle project and I am having UART communication issues between the BQ76PL455EVM and the TMS570LS1224. I have tried to follow the steps from a similar forum posting (https://e2e.ti.com/support/power_management/battery_management/f/1002/t/668626?BQ76PL455EVM-No-UART-response).
Main Issues:
-No UART response when I send anything. I am trying “81 00 0A 00 2E 9C” and expect "00 00 00 00" and the TX on the EVM just stays on high. It works if I use my PC GUI.
-No response or return value when I try to read device ID
//nRead = ReadReg(nDev_ID, 10, &wTemp, 1, 0);
My setup is the same as the link, with the exception that I did not use a voltage converter so I am doing 3V3 directly from the TMS to the EVM.
The code sample is attached in the above link.
Thanks in advance!