This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,all:
Now I do a work about port a SRIO software example(2677.K1_STK.7z) which
worked well on EVMC6678 to the platform DSPC-8681E with four C6678s.
The key point is about DDR3 config or init.
And the difference between EVMC6678 and DSPC-8681E is frequence of input
refclk.
On C6678EVM DDR input refclk is 66.667MHZ(learned from 5852.TMDSEVM6678L_Technical_Reference_Manual_2V01_0320.pdf):
On DSPC-8681E DDR input refclk is 166.67MHZ(learned from 6131.DSPC-8681E HW User Manyal_V0.3_20120621.pdf):
Meanwhile,the source code of C6678EVM DDR init in SRIO example is below:
//DDR init 66.66667*20/1= 1333
KeyStone_DDR_init (66.66667, 20, 1, NULL);
In the above statement, 66.66667 is the DDR input refclk frequence.PLLM = 20,
and PLLD is 1.1333 is the work frequence of DDR3 which is on EVMC6678.So,If you
want to get 1333MHZ,you must calc like this:66.66667*20/1= 1333. So,you get PLLM
=20,PLLD = 1.But Is PLLM = 40 PLLD = 2 ok?And Are others value ok only if the value
of PLLM/PLLD is 20? I think so.Isn't wright?
So,According to my guess above.When I port the source code from EVMc6678 to DSPC8681E.
I modify the source code about DDR init like below:
KeyStone_DDR_init (166.67, 8, 1, NULL);
Because 166.67*8/1 = 1333.36MHZ. So I set those values like above.
But,when I run that code on DSPC8681E board. I cannot pass the memory test of DDR.
I find that the value which I read from the DDR in some address is not the value that
I write into the same address of DDR.
Since,I don't know where I make mistake? How can I config DDR3 registers on DSPC-8681E
considering that its DDR input refclk is 166.67MHZ not 66.667MHZ and the target frequence
of DDR3 on DSPC-8681E is 1333MHZ?
Kindly Regards!
Hi David,
Remember that there is a /2 in the DDR PLL after you program the PLLM and PLLD.
DDR3-1333 means a DDR interface clock of half that speed (~666MHz). This does not affect your programmation of the PLLM/PLLD values from your post, but just something you should be aware of.
First, KeyStone_DDR_init (166.67, 8, 1, NULL); should configure the DDR3 PLL correctly for DDR3-1333 if 166.67MHz is the reference clock. But when you ported the sequence to the DSPC platform, did you also make sure your SDCFG and SDRAM timing registers are programmed in accordance with the memory parts on that board? Do they have the same row/column sizes? Are all the timing parameters the same? I would check the memory device datasheet for that.
Second, is it possible for you to probe the DDR3 CLK on the DSPC board? I am not too familiar with that platform, but if there a probe point that you can tap and verify the correct clock (~666MHz) then that would settle the question of correct clock configuration.