Other Parts Discussed in Post: ADS1118

Thermal noise in analog design is almost always parasitic and should be avoided at all costs. Input filtering, PCB layout and grounding are paramount to good analog system designs, but you’ll always find some amount of thermal Johnson-Nyquist and flicker noise in an analog system.

An additional noise source, quantization noise, can actually outweigh the noise from thermal and other noise sources. Quantization occurs when the signal converts from analog to digital.

Figure 1 shows the quantization noise resulting from an extreme example of a 4-bit analog-to-digital converter (ADC) digitizing a sine wave.

Figure 1

When you use a ruler to measure an object, you actually count the marks on the ruler to measure the size of the object, right? What happens when the object’s size is between two markings? If you’re forced to make a decision between two of the ruler marks, you’ll choose the one that’s closest to the actual size of the object. The difference between that, and rounding to the nearest tick mark, is a physical representation of quantization noise.

All ADCs do this with the voltages connected to their inputs. They look at the signal and approximate the actual voltage into a finite number of steps. The number of usable steps in an ADC determines the resolution.

The noise shaping characteristics of high-precision delta sigma ADCs generally minimizes thermal and flicker noise. In the case of 16-bit and lower devices, thermal noise can become much less than the error due to the approximation of the signal.

In ADCs like these, you may find almost no change in digital codes at low data rates. We almost exclusively see quantization error in the actual signal as the device reads it.

That’s enough performance for many applications. However, we can improve quantization noise and achieve better than 16-bit resolution, even though we only have a 16-bit ADC.

How? Add noise, of course!

By adding statistically random or Gaussian noise to the input of an ADC, the LSB will start flickering. This is known as dithering. If we average the flickering over a series of readings, the result is closer to the actual value than a lower noise front end that is causing no change in codes.

A great way to do this is to increase the sample rate of a 16-bit ADC until the LSB begins to flicker. Figure 2 provides an example of this. The increased noise allows averaging to create a more accurate result, while still delivering the same throughput.


Figure 2

Performing the averaging math is simple. For example, when using the 16-bit ADS1118 at 8 samples-per-second, most systems yield a stable result with no digital code changes. In this case, our error is dominated by quantization noise. However, if the device runs at 128 samples-per-second, there is enough noise to create digital codes varying between each other.

To average these 16 samples in an MCU, accumulate all of the results as they come in. The division is easy after that because the number of samples is a power of 2. Simply rotate the result to the right four times. These extra 4 bits are usable resolution. Same data rate, with more resolution because of a little noise.

How cool is that?!?

Anonymous
  • Hi Mike,

    Get your article, but I didn't know your mail address, so I have to write to you here.

    I have another question about your applicaiton datasheet of ADS1118(Precision Thermocouple Measurement with the ADS1118), you mensioned how to get the actual temperature of thermocouple by using tempearture and voltage lookup table, and you also said that the entries of the lookup table 16 and 32 for k-type thermocouple would be enought for presion and draw a comparasion figure for your idea. My question is what is the detailed point for 16 and 32 entries table? I think these points should be scientific and I also didn't the details from TI website, so I have to write to you. Could you send the details to me? thanks very much.

    My mail address: wylinder@163.com

  • Golden Warrior,

    To your comment, "abandoned by the rotation to the right four times, how can it be used if the four bits still dithering?"

    The short answer is because the final output rate of the data is much slower and effectively averaged. If you think about the statistical nature of the unmodified 16-bit result for DC signals between two codes you should notice that the LSB should tend toward whichever code is closest to the actual signal. This will happen proportionally to how close the signal actually is to the code. The process of oversampling (adding and rotating right), while actually smooth out some of the noise added for the dither and will actually provide a very stable result. However if the dithering noise is too high, it is possible that those extra bits will be toggling. For gaussian noise, every averaging of two datapoints into one slower data point results in a factor of roughly sqrt(2) reduction in noise.

    For your second question, "is there enough noise to create digital codes varying between each other, if the device runs at 128 samples-per-second?"

    It really depends on how noisy the input signal is. If the noise of the input signal is very small, a sample rate of 128SPS may not be sufficient to cause toggling of the LSB. One option, as long as your input range can allow it, would be to increase the gain of the PGA in front of the modulator. This will double the size of the signal entering the modulator, and also double the noise coming in from the outside. This might increase the noise just enough to use the dither at 128SPS. For the ADC alone (shorted inputs on a clean design), you should see a peak-to-peak noise of almost 1LSB at gain of 1. This wont quite be enough noise use the technique, but if you increase the gain, you'll cut each LSB step size in half, which should just barely provide enough bits toggling to use the technique. 128SPS is right on the edge of having enough noise for this technique.

  • Hi,Mike,

    "The ADS1118 can perform conversions at rates up to 860 samples per second", is there enough noise to create digital codes varying between each other, if the device runs at 128 samples-per-second?

    Under which sample rates yield a stable result with no digital code changes?

  • Glad to read your share. Here are two quetions?

    1 Why is it told that "the result is closer to the actual value than a lower noise front end that is causing no change in codes"?

    2"These extra 4 bits are usable resolution. Same data rate, with more resolution because of a little noise", As the four bits are to be

    abandoned by the rotation to the right four times, how can it be used if the four bits still dithering?  

  • It's great to see this pop up every so often. FYI, my first encounter with it was in 1990, discovered while browsing the university library stacks. Found this intriguing article in a Physics Journal from the 1970s that described this method.