Browse By Tags

  • ADS1118EVM: TI Web GUI Data Capture Not drawing line between points, data is seemingly invisible.

    Part Number: ADS1118EVM
    Other Parts Discussed in Thread: ADS1118

    Tool/software:

    My device connects fine, when I attempt to capture data on the correct channel (I tried all of them just in case) the time domain window doesn't have any lines connecting…

  • ADS1118: About K-type Thermocouple measurement accuracy

    Part Number: ADS1118

    Tool/software:

    Hi team,

    Our customer measured error rate between the ADC digital output and K-type thermocouple input in followed below application note.
    In this mesurement, we use register setteing noted in p5.

    www.ti.com/.../sbaa354a…

  • ADS1118: About Erectric characteristic value

    Part Number: ADS1118

    Tool/software:

    Hi team,

    Could you tell us below information about electric characterictic value.

    1,Minimum Differential input impedance @FSR=±0.256V
    2,Maximum Differential input impedance @FSR=±0.256V

    3,typical and maximu…

  • ADS1118: ADS1118IRUGR

    Part Number: ADS1118

    Tool/software:

    Hi there,

    We want to read Analog voltage ( 0-5V) which comes from display interface.

    Can we use voltage divider as 3.3V to AIN1 channel for the part : ADS1118IRUGR ?

    Ref Image:

    Please, Advise.

  • TIPD109: I2C/SMBus of ADS1118

    Part Number: TIPD109
    Other Parts Discussed in Thread: ADS1118, ADS1115, ADS112C04

    Tool/software:

    Hi,

    Because ADS1118 is SPI interface, I would like to know whether there is alternative part with I2C or SMBus part for TIDA109 application?

    Thanks and Best…

  • ADS1118-Q1: ADC for Electro-impedance spectroscopy(EIS) application

    Part Number: ADS1118-Q1
    Other Parts Discussed in Thread: ADS1118,

    Tool/software:

    Hi Team,

    Customer is trying to design ADS1118 as ADC for EIS application that measures the impedance between the fuel-cell stacks. So they need the application note for EIS…

  • ADS1118: RTD vs thermcouple

    Part Number: ADS1118
    Other Parts Discussed in Thread: ADS1220

    Tool/software:

    Hello  All,

    I was wondering if it is  possible to use a RTD instead of a thermocouple with this chip or  are there other chips available able to do the same job as the ADS1118…

  • ADS1118: The ADC promoted

    Part Number: ADS1118

    Tool/software:

    Hi,

    We need to choose the ADC for the single sampling, and the spec. request as below:

    1. The input voltage range -100mV ~ 100mV;

    2. The temperature accuracy +/- 0.05%;

    3. The 2 channels total response time less than…

  • TAS2563: Device tree configuration for Microphone

    Part Number: TAS2563
    Other Parts Discussed in Thread: TAS2562, TAS2781, AM623

    Tool/software:

    Hi, 

    I'm using TAS2563 codec for audio, I'm using TAS2562 driver. I have added device tree configuration to use the codec for speaker and can utilize "aplay…

  • M2-CC3301: am62x: cc33xx_probe fail

    Part Number: M2-CC3301

    Tool/software:

    Hi,

    I am trying to integrate cc3301 in the custom AM62xx.

    getting below error while loading the driver, please give suggestion

     $ sudo dmesg
    [  118.702689] cc33xx_sdio mmc2:0001:2: sdio PM caps = 0x1
    [  118.702755] cc33xx_sdio…

  • ADS1118: Four channels with J-type thermocouple temperature

    Part Number: ADS1118
    Other Parts Discussed in Thread: TIPD109, ADS114S08

    Tool/software:

    Hi team,

     we check some E2E thread about the ADS1118 use case of hot electric puppet . like TIPD109 for one channel with K-type.

     Now customer have 4channels J-type demand…

  • ADS1118: ADS1118IDGSR

    Part Number: ADS1118
    Other Parts Discussed in Thread: LMR51450

    Tool/software:

    Hi Sir,

    My self i'm Sandeep,

    Here i'm using the LMR51450 Switching regulator for 12V to 5VDC conversion, and i'm giving this switching regulator supply to ADS1118IDGSR,…

  • ADS1261: appropriate ADC for temperature measurement(pt-100 and TC k-type)

    Part Number: ADS1261
    Other Parts Discussed in Thread: ADS124S06, ADS1118

    Tool/software:

    Dear Technical Support Team,

    Could you suggest appropriate and precise ADC?

    ①Pt100    : Error ±1          12bit or more

                     1 digit under 0.1℃

    ⇒ADS1261 or ADS124S06 are…

  • ADS1118: NOP Field Indicates Invalid Data

    Part Number: ADS1118

    For part ADS1118IDGST, in Page 27 of datasheet (Table 7) NOP field = 00 was interpreted as invalid data.  I have recently encountered this response in an application and been wondering what does that actually mean?  Thanks!

    Link to…

  • ADS1118: PGA internal block diagram

    Part Number: ADS1118

    Hi,

    Can you provide the PGA internal block diagram of ADS1118?
    Looking at the datasheets of other TI PGA products, it seems that the internal block diagrams are disclosed.

    Thanks,

    Conor

  • ADS1118: How to calculate Ccm if the input of the ADC is single ended for anti-aliasing filter?

    Part Number: ADS1118

    Is Ccm calculated the same way as Cdiff in differential input sigma-delta ADC?

    Since the input is single ended, although Ccm is connected between input to GND. I think it's still acting as a differential capacitor since the signal…

  • ADS1018: Suitable ADC required to monitor 3-phase AC Load Using Current Transformer

    Part Number: ADS1018
    Other Parts Discussed in Thread: ADS1118, , ADS131M04, ADS131M03, ADS131E04, MSPM0G1107, ADS131M08, ADS131M06

    Hi,

    We need to Monitor the 3-phase Load Current using three Current Transformer(CT) for each phase. We need SPI communication…

  • ADS1118: Need Linux driver and demo application for ADS1118

    Part Number: ADS1118
    Other Parts Discussed in Thread: ADS124S08

    Hello,

    Currently I need to interface ADS1118 to linux based system.

    I need Linux driver for ADS1118 and also It will be good to have some reference example application code for it.

    Could you…

  • ADS1118EVM: ADS1118EVM

    Part Number: ADS1118EVM
    Other Parts Discussed in Thread: ADS1118, ADS1115

    Hi,

    I am trying to get a PIC18F87J90 controller on a Microchip development board to drive ADS1118EVM with SPI. The issue is that I do not see it convert after the configuration…

  • ADS8689: spec check

    Part Number: ADS8689
    Other Parts Discussed in Thread: ADS1118, ADS1260

    Hi

    The customer has a problem with the ADS8689. If the input terminal needs to be reset to 0 ohm, the problem can be corrected.

    ADS8689 PIN 7,8 SHORT

    The software does not receive…

  • ADS1119: ADS1119 ADC Address Mixed Up

    Part Number: ADS1119
    Other Parts Discussed in Thread: ADS1118

    I had ADS1119 in one of my project. I noticed that I can read the AIN0 data when I used AIN3 address, and AIN0 address gives AIN3's data. I have tried to troubleshoot by myself, I couldn't…

  • ADS1118: possible to change differential input resistor value ???

    Part Number: ADS1118

    Hello~

    There is a Figure 50. Two-channel thermocouple measurement system.

    Can I change resistor value from 500R to 50R? 

    does it affect to thermocouple measurement ? 

  • ADS1118: how to convert thermocouple input millivolt to degree celcius ????

    Part Number: ADS1118

    Hello~

    I'm testing ADS1118 with arduino mega and ADS1118-master library.

    Test circuit is referenced from Fig.50. Two-Channel Thermocouple Measurement System in ADS1118 datasheet.

    K-type thermocouple, FSR = ±0.256V (7.8125 uV resolution…

  • ADS1118: The config register bit0 read back 0

    Part Number: ADS1118

    Hi experts,

    Good day! My customer is using ADS1118 in BMS. They encounter an issue in testing SPI comm. RD wrote 1 to bit0, but some times read back is 1, some times read back is 0.

    According to datasheet, bit0 should always reads…

  • ADS1118: 1

    Part Number: ADS1118

    Hello,

    For lab check of part: ADS1118 Ultrasmall, Low-Power, SPITm-Compatible, 16-Bit Analog-to-Digital Converter with Internal Reference and Temperature Sensor

    I will appreciate your answers for the following question:

    1. The component…

1 2 3 4 5 »