This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LSF0204: Why does 3.3 V IO have a voltage drop?

Part Number: LSF0204

Hi TI,

Could you please let me know why PCIE_33_RST_N has a voltage drop?

I did the same test with TXS0104 but it didn't observe the below weird waveform.

Please refer to the below schematic/block diagram and waveform.

Schematic of LSF0204

Waveform: Voltage drop w/LSF0204

Waveform: NO Voltage drop w/TXS0104

Block Diagram (Simplified)

Thank you.

Best Regards,
Seunghwan Lee.

  • The LSF is a passive switch. The high-level voltage is generated only by the 10 kΩ pull-up resistor. The voltage is lower because some component is pulling the line low (with about 20 kΩ).

  • Thanks for your comment.

    1. As I know LSF has FET but I have no idea why it's a passive switch. Do you mean is that acting like a passive switch?

    2. I'm just wondering why it's 20 K ohm.

    3. 'Some component' means Network Interface Card or something?

    Could you please explain in more detail?

    4. Some NICs have an internal pull-up on the PCIE_RESET_N line, but we don't know the value. It was also dropped.

     

  • 1. The FET is a passive switch. When any input is low, the gate-to-source voltage of the FET is large enough, and it connects the pins on both sides.

    2. The 10 kΩ pull-up and the unknown pull-down form a voltage divider. The resulting voltage is about 2 V. (If there are other pull-ups on the line, then the pull-down also is stronger.)

    3. I don't know. I just see the effect.

  • I thought you were talking about FET as a passive component. Sorry, I misread a word as 'a passive switch'.

    Then, why TXS0104 does not cause a voltage drop? It also has an internal 10 K pull-up resistor.

  • here, "passive" means that the I/Os are not buffered.

    I do not know why the TXS behaves differently; the LSF and TXS have the same architecture (the TXS just adds internal pull-ups and edge accelerators).

  • Thanks for your answer.

    I've tested without NIC and It was the same result.

    It doesn't have anything to do with NIC.

    So, please ignore the block diagram.

    LSF0204; Added an external 10K pull-up on PCIe_33_RST_N (Still has a large voltage drop (without NIC))

    TXS0104(Internal 10K pull-up); No external 10K pull-up on PCIe_33_RST_N (without NIC)

    Still wondering why LSF has a large voltage drop even though there's no connection on the B side's IO.

  • Hi Seunghwan,

    When you say no connection on the B side's I/O, do you mean the PCIE connector is disconnected as well?

    Note that your schematic seems to indicate the device has no outputs at all, as PCIE_RST and PCIE_33 seems to be both going into the device. Please help confirm for bus contention as the TXS case also seems to be dropping after a longer while, thanks.

    Best Regards,

    Michael.

  • Hi Michael,

    Thank you for your comment.

    No connection on the B side's I/O means the PCIE connector is disconnected.

    There's nothing connected to B-side.

    I wonder why LSF0204 has a voltage drop on B-sides at the first waveform.  

    Because the TXS series does not have a voltage drop. (Please refer to the above capture, RED circle)

    It's okay to be dropping after a longer while.

    Thank you.

    Best Regards,

    Seunghwan Lee.

  • Hi Seunghwan,

    Note that the TXS has edge accelerators which speeds up the edges. Would the host happen to have internal pull-downs? 

    Best Regards,

    Michael.

  • Yes, the host has an internal pull-down.

    But I don't know the specific value.

    I knew the TXS series have an edge accelerator. 

    But I thought the edge accelerator doesn't affect dropping voltage.

    If the level translator has edge accelerators, it influences to the voltage drop?

  • Hi Seunghwan,

    No, the edge accelerators may speed the rising edge while working with the internal 10K of the TXS device. 

    It seems the 10K is stronger than the host's pull-down. However, the LSF do not have pull-ups. You may add pull-ups on A1 to help pull-up, thanks.

    Best Regards,

    Michael.

  • Thank you, Michael.

    It helps a lot!