Part Number: EVM430-F6779 Other Parts Discussed in Thread: MSP430F6779 , MSP430I2040 , MSP-EXP430F5529LP , MSP-ISO
Tool/software: Code Composer Studio
Hello,
We aim to deploy the code as it generated by EMDC on to MSP430F6779 EVM.
We would like…
Part Number: DCA1000EVM This information applies to any of the mmWave sensor BOOST EVMs
As described in the mmwave studio User's Guide Section "3 Using the DCA1000 EVM for capturing the raw ADC data", after 1GB of capture, a new file will be created…
Part Number: AWR1843 Other Parts Discussed in Thread: UNIFLASH A common question regarding uniflash is how not to erase entire flash when flashing new binaries.
For example, a common use case is to store calibration coefficients in Flash. So, let's…
Part Number: TPS63020
Hi,
I am troubled that the phase margin of TPS63020 can only be about 30 deg.
Please tell me how to improve the phase margin. Also, please tell me how much phase margin is required.
Best Regards,
Hasegawa
Hello Users,
TI Resource Explorer upgraded to version 4.0 recently and some of the links referencing Resource Explorer Projects and Labs are no longer working. This is currently a known issue and TI is working to address this.
In the meantime, one…
FAQ: Logic and Voltage Translation > Input Parameters >> Current FAQ
The most common example of this question comes from the fact that Standard Logic devices are specified at 1.65V, 3V, and 4.5V, however most engineers use our devices at 1.8V, 3.3V…